20
Downloads
0
Downloads of v 5.5.0
2026-03-04
Last published
mplab-x-sdk
5.5.0
Welcome to the MPLAB X SDK! This software development kit contains documentation, sample code, and precompiled libraries for developing a Plugin for MPLAB X IDE, or a standalone application of the MDBCore API. Please use developers forum on Microchip Website for any help/suggestions on SDK.
To install mplab-x-sdk, download this package and open it in IDE.
Supported Products: MPLAB X
Release Notes
What's New in v5.05
REMINDER :
New Project format – The new project format in v5.00 and greater supports packs which contain versioned device information. Packs can be found under \v5.xx\packs.
Projects created in or updated to v5.00 or greater are not backward compatible to v4.xx. When you open a project created prior to v5.00, a message displays that it will upgrade the project to the current project version. If you choose Yes, the project will be upgraded to the current version and the project can no longer be opened with the earlier version of the IDE. If you choose No, you cannot save any modifications to the project in v5.00 or greater. You must make any changes in v4.xx or install a plugin. If you upgraded a project to v5.xx but need to revert a project back to v4.xx, install a plugin in MPLAB X IDE, under Tools>Plugins>Available Plugins>Save As v4.xx Project. Once that plugin is installed, you can save your project in the older version by selecting Tools>Embedded>Save as MPLAB X v4.xx Project.
MPLAB Snap – New low-cost in-circuit debugger/development programmer tool.
Owners
Authors
Copyright
Microchip
Tags
Dependencies
-
- No dependencies.
Version History
| Version | Downloads | Last updated | Approved |
|---|---|---|---|
| mplab-x-sdk 6.30.0 (latest stable) | 9 | Tuesday, March 3, 2026 | yes |
| mplab-x-sdk 6.25.0 | 1 | Tuesday, March 3, 2026 | yes |
| mplab-x-sdk 6.20.0 | 1 | Tuesday, March 3, 2026 | yes |
| mplab-x-sdk 6.15.0 | 2 | Tuesday, March 3, 2026 | yes |
| mplab-x-sdk 6.10.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 6.5.0 | 3 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 6.0.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.50.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.45.0 | 1 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.40.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.35.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.25.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.20.0 | 2 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.15.0 | 1 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.10.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.5.0 (this version) | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 5.0.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 4.20.0 | 0 | Wednesday, March 4, 2026 | yes |
| mplab-x-sdk 4.5.0 | 0 | Wednesday, March 4, 2026 | yes |